Create a local message display
Create a local message display that prompts the operator about the information of a process or what to do next.
To create a local message display
- In theGraphics Displayeditor, selectObjects >Advanced > Local Message Displayor drag
from the toolbox. - Drag the cursor to position and draw a rectangle the general size and location you want the display to be.
- Double-click the display to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the display looks, the message file to use with the display, and its tags.
Provide Feedback