Linear Gauge Properties - Threshold tab
The following table shows options under
Value range settings
of the
Threshold
tab.Options | Description |
|---|---|
Minimum value | Enter the minimum value of the linear gauge. This is only available
if Use variable is cleared. |
Maximum value | Enter the maximum value of the linear gauge. This is only available
if Use variable is cleared. |
Use variable | Select this check box if you plan to use the Minimum and
Maximum connections on the Connections tab for the
linear gauge's value range. |
The following table shows options under
Threshold settings
of the Threshold
tab.Options | Description |
|---|---|
Normal operating range color | Select the color for the normal operating range on the linear
gauge. |
Use variable | Select this check box if you plan to use the High High ,
High , Low , and Low Low connections on the
Connections tab for the linear gauge's thresholds. |
Thresholds: High High, High, Low, Low Low | The current value is compared against the values of the thresholds.
To enable any threshold, select the associated check box. The
thresholds' check boxes are only available if Use variable is
cleared.Thresholds trigger visual alerts when values reach or cross predefined
boundaries to help maintain system stability. For example, when a process variable
crosses a threshold, it indicates an issue or deviation from the desired operation. You
must respond with actions to prevent deviations and maintain optimal performance.
TIP:
Only enabled thresholds
can show their threshold lines on the sparkline. |
Inactive | Select the color for the threshold on the linear gauge when the
current value does not reach it. |
Active | Select the color for the threshold on the linear gauge when the
current value reaches or crosses it.
TIP:
The active threshold color determines the threshold
lines' color on the sparkline. |
Blink | Select this check box to enable the alarm indicator on top of the
linear gauge to blink when the current value reaches or crosses a
threshold at runtime. |
The following table shows options under
Control limit settings
of the
Threshold
tab.Options | Description |
|---|---|
Control limits: High High, High, Low, Low Low | The current value is compared against the values of the control
limits. To enable any control limit, select the associated check
box. The control limits' check boxes are only available if Use
variable is cleared.Control limits are predefined limits that help ensure safe and
efficient operations by preventing alarm conditions. These limits help maintain process
quality by monitoring critical variables, such as temperature or pressure, and adjusting
operations to prevent deviations that might lead to defects, safety hazards, or
inefficiencies. For example, if the ideal temperature of a reactor is 100°C, the control
limits might be set at 95°C and 105°C. If the temperature goes beyond these limits, the
PID controller will take corrective actions to bring back the variable within the
acceptable range. |
Use variable | Select this check box if you plan to use the Control limit High
High , Control limit High , Control limit Low ,
and Control limit Low Low connections on the
Connections tab for the linear gauge's control
limits. |
Control limit icon size | Select the icon size for the control limits. |
Within control limit color | Select the color for the control limits when the current value does
not reach or cross the control limit. |
Beyond control limit color | Select the color for the control limits when the current value
reaches or crosses the control limit. |
Provide Feedback