Linear Gauge Properties - Sparkline tab
The following table shows the options of the
Sparkline
tab of Linear Gauge
Properties
.Options | Description |
|---|---|
Enable sparkline | Select this check box to show the sparkline, a simple line-chart that
appears adjacent to the linear gauge. The sparkline shows the
history for the current value, providing a visual representation of
the recent trend within a time duration. |
Bar width (vertical linear gauge) or Bar height
(horizontal linear gauge) | Enter the number of pixels for the width or height of the linear
gauge bar, depending on whether the linear gauge is vertical or
horizontal.
TIP:
To hide the bar, set the bar
width to zero.
|
Line width | Select the number of pixels for the width of the line itself.
TIP:
The value indicator color determines the line color of
the sparkline.
|
Time duration (second) | Enter the sparkline time duration in seconds, ranging from 5 through
600. |
Grid line style | Select whether to show the grid lines or the style of the grid
lines. |
X-axis grid lines (vertical linear gauge) or Y-axis grid
lines (horizontal linear gauge) | Select the number of vertical grid lines or horizontal grid lines,
depending on whether the linear gauge is vertical or horizontal.
TIP:
The number of major ticks on the scale
determines the number of grid lines in the sparkline: horizontal grid lines if the gauge
is vertical, and vertical grid lines if the gauge is horizontal.
|
Grid line color | Specify the color of the grid lines. |
Show threshold lines | Select this check box to show the threshold lines.
TIP:
Only enabled thresholds
can show their threshold lines on the sparkline.
The active threshold color determines the threshold
lines' color on the sparkline. |
Provide Feedback