Linear Gauge Properties - Display tab
The following table shows options under
Current value
of the Display
tab.Options | Description |
|---|---|
Show current value | Select this check box to show the current value below or above the
linear gauge, depending on whether it's vertical or horizontal. |
Field length | Select the character length of the current value. |
Decimal places | Select the number of digits to show after the decimal point. |
Font , Size , and Color | Select the font type, size, and color for the current value. |
Show engineering unit | Select this check box to show the engineering unit of the current
value. |
Use variable | Select this check box if you plan to use the Unit connection
on the Connections tab for the engineering unit. |
Font , Size , and Color | Select the font type, size, and color for the engineering unit. |
The following table shows options under
Target
of the Display
tab.Options | Description |
|---|---|
Enable target | Select this check box to show the target value on the linear
gauge. The target value is the desired value that the process aims to achieve.
The setpoint is more commonly associated with immediate control actions within a PID
system, whereas the target value can be used for a broader goal or benchmark that the
process aims to achieve over time. For example, in a ramping process, the target value
can be the final temperature you want to achieve after a certain period, such as 600°C.
The system will gradually adjust the setpoint to reach this target value. |
Use variable | Select this check box if you plan to use the Target value ,
High deviation , and Low deviation connections on
the Connections tab for the linear gauge's target value. |
Target value | Specify the target value. This is only available if Use
variable is cleared. |
Target color | Select the color for the target value indicator. |
High deviation | Specify the high deviation value around the target value. This is
only available if Use variable is cleared.High deviation occurs when the process
variable (PV) is above the target value.
High deviation and low deviation define a tolerant range
around the target value. |
Low deviation | Specify the low deviation value around the target value. This is only
available if Use variable is cleared.Low deviation occurs when the PV is below the
target value. High deviation and low deviation define a tolerant range around
the target value. |
Expected range color | Select the color for the expected range between the low and high
deviations around the target value. |
To enable the setpoint, select
Enable setpoint
.- With setpoint enabled, configure theSetpoint valueconnection on theConnectionstab. The setpoint uses the same color as the target value indicator.
- The setpoint is the desired value that you want the PV to reach or maintain. For example, in a PID controller, the setpoint represents the reference or goal for the controlled PV, such as temperature, pressure, or flow rate. The setpoint is used for immediate control actions to maintain a specific value, whereas the target value is used for planning or achieving the final goal for the entire process after a series of adjustments or steps.
Provide Feedback