Linear Gauge Properties - Connections tab
The following table shows the options of the
Connections
tab of Linear Gauge
Properties
.Options | Description |
|---|---|
Value | Specify a tag, expression, or numeric value that will define the
current value for the linear gauge. |
Minimum | Specify a tag, expression, or numeric value that will define the
minimum value of the linear gauge. |
Maximum | Specify a tag, expression, or numeric value that will define the
maximum value of the linear gauge. |
Unit | Specify a tag, expression, or numeric value that will define the
engineering unit for the current value. To use this connection, make
sure to enable Show engineering unit on the Display
tab. |
High High | Specify a tag, expression, or numeric value that will define the High
High threshold. |
High | Specify a tag, expression, or numeric value that will define the High
threshold. |
Low | Specify a tag, expression, or numeric value that will define the Low
threshold. |
Low Low | Specify a tag, expression, or numeric value that will define the Low
Low threshold. |
Target value | Specify a tag, expression, or numeric value that will define the
target value. To use this connection, make sure to enable target on
the Display tab. |
High deviation | Specify a tag, expression, or numeric value that will define the high
deviation for the target value. |
Low deviation | Specify a tag, expression, or numeric value that will define the low
deviation for the target value. |
Setpoint value | Specify a tag, expression, or numeric value that will define the
setpoint value. To use this connection, make sure to enable setpoint
on the Display tab. |
Control limit High High | Specify a tag, expression, or numeric value that will define the
control limit High High. |
Control limit High | Specify a tag, expression, or numeric value that will define the
control limit High. |
Control limit Low | Specify a tag, expression, or numeric value that will define the
control limit Low. |
Control limit Low Low | Specify a tag, expression, or numeric value that will define the
control limit Low Low. |
Provide Feedback