Linear gauge components
This is an example of a linear gauge with a table explaining the components on it.
Components | Description |
|---|---|
![]() | Alarm indicator. It is displayed when the process variable reaches or
crosses a threshold. |
![]() | Target value and tolerant range |
![]() | Setpoint. It is the desired target value for the process
variable. |
![]() | Control limit. It is the predefined limit that helps ensure safe and
efficient operations by preventing alarm conditions. |
![]() | Value indicator |
![]() | Threshold. It triggers visual alerts when values reach or cross
predefined boundaries. |
![]() | Threshold line |
![]() | Grid line |
![]() | Line |
![]() | Current value and engineering unit |
![]() | Time duration |
![]() | Bar width |
Provide Feedback