Create a Latched push button
Use the
Latched
push button object to create a button with a latched and unlatched state. This type of button is useful for starting a machine or process.For example, use the
Latched
push button when you want the Value connection to start a process within a programmable logic controller (PLC) and remain set until the process is completed. You can also use a latched
push button when you have a PLC with a long program or long update times.To create a Latched push button
- In theGraphics Displayeditor, selectObjects > Push Button > Latchedor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks, how to unlatch the button, and its tags.IMPORTANT:Do not use push buttons for emergency stops. Emergency stop buttons must be hard-wired.
TIP:
Use the Handshake connection to signal that the program has read the Value connection.
The
Latched
push button sends a value to the data source when pressed, and retains this value until reset by the Handshake connection.Provide Feedback