Create a Language Switch button
At runtime, the
Language Switch
button changes the language of the application to the language specified by the button.To create a Language Switch button
- In theGraphics Displayeditor, selectObjects > Advanced > Language Switch Buttonor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks and, what language it will switch the application to.
Provide Feedback