Options on the Timing tab of the Key Button Properties dialog box
The following table shows the options on the
Timing
tab of a Key
button's Properties
dialog box.Options | Descriptions |
|---|---|
Auto repeat rate | Specifies the number of times per second a button press is registered when the button goes into auto repeat mode. Select 0 if you don’t want to use auto repeat. |
Auto repeat delay | Specifies the length of time the button has to be pressed and held down before auto repeat starts. |
Provide Feedback