Create a Goto Display button
At runtime, the operator can press a
Goto Display
button to open the graphic display assigned to the button.
TIP:
The operator cannot use this button to open Replace displays if display change is currently controlled remotely. But the operator can still open On Top displays (with or without the
Cannot Be Replaced
option).To create a Goto Display button
- In theGraphics Displayeditor, selectObjects > Display Navigation > Gotoor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want theGoto Displaybutton to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks and the display to go to.
Provide Feedback