Create a Goto Configure Mode button
At runtime, the operator can use a
Goto Configure Mode
button to open the terminal's Configure Mode. When the operator presses the button, the application stops and the main Configure Mode
dialog box opens.To create a Goto Configure Mode button
- In theGraphics Displayeditor, selectObjects > Advanced > Goto Configure Modeor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback