Create a gauge
The gauge is a semi-circle with a needle and range of values that represents a traditional meter or dial.
Use the gauge object to display a control’s value at the data source. The gauge’s needle moves around the dial to show the changing value. You can configure thresholds for the gauge to alert the operator to error conditions.
To create a gauge
- In theGraphics Displayeditor, selectObjects > Gauge and Graph > Gaugeor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the gauge to be.
- Double-click the gauge to open itsPropertiesdialog box.
Provide Feedback