Create a Display Print button
At runtime, the operator can use the
Display Print
button to generate a screen print of the visible portions of all the displays that are currently open, including portions of other Windows applications that are visible. The screen print is printed on the printer connected to the computer running the application.To create a Display Print button
- In theGraphics Displayeditor, selectObject > Advanced > Display Printor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback