Create a display list selector
Use the display list selector to show a list of graphic displays that the operator can choose from. The operator can scroll through the list and select a graphic display.
The operator can scroll through the list and select displays using key buttons or by using the arrow keys and
Enter
key on a keypad or an external keyboard.
TIP:
- The operator cannot use the display list selector to open Replace displays if display change is currently controlled remotely. But the operator can still open displays of the type On Top (with or without theCannot Be Replacedoption).
- Users cannot navigate through the Display List Selector by holding the Up or Down key on a terminal running FactoryTalk View ME Station version 6.10.00.To avoid this problem, in FactoryTalk View ME Station, go toTerminal Settings>Input Device>Keyboard/Keypadand change the value forRepeat Rateto 2 or greater.
To create a display list selector
- In theGraphics Displayeditor, selectObjects > Display Navigation > Display List Selectoror drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the selector to be.
- Double-click the selector to open itsPropertiesdialog box.
Provide Feedback