Create a Close Display button
At runtime, the operator can press a
Close Display
button to close the graphic display that the button is on.To create a Close Display button
- In theGraphics Displayeditor, selectObjects > Display Navigation > Closeor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback