Create a Clear Audit Trail button
Use the
Clear Audit Trail
button to clear the audit log file, audit trail list, and audit trail RAM cache.To create a Clear Audit Trail button
- In theGraphics Displayeditor, selectObjects > Advanced > Audit > Clear Audit Trailor drag
from the toolbox. - Drag the mouse to draw a rectangle of the general size and in the general location you want the button to be.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks.
Provide Feedback