Create a bar graph
Use the bar graph object to show a control’s value at the data source. The bar graph increases or decreases in size to show the changing value. You can configure thresholds for the bar graph to alert the operator to error conditions.
To create a bar graph
- In theGraphics Displayeditor, selectObjects > Gauge and Graph > Bar Graphor drag
from the toolbox. - Drag the mouse to position and draw a rectangle the general size and location you want the bar graph to be.
- Double-click the bar graph to open itsPropertiesdialog box.
Provide Feedback