Application settings
In
FactoryTalk View Studio
, use the Options
dialog box to configure settings that apply to all applications. The following table shows options on the Settings
tab of the dialog box.
Option | Description |
|---|---|
Auto-open Property Dialog | Select the check box to automatically open the graphic object Properties dialog box when you release the mouse button after drawing the object.If you clear the check box, you can double-click the object, or right-click the object and then select Properties from the context menu to open the Properties dialog box. |
Use the legacy default color | Select this check box to use the legacy default color for graphic objects. |
Exclude referenced tags from scanning when object is invisible | Select this check box to take invisible objects' associated tags off scan, except for the visibility expression. By default, this check box is selected in new applications created in version 14.00 or later. For those objects to remain invisible on the display and their tags on scan, we recommend that you set the objects' position to a negative value so that they are outside of the display frame or configure their appearance so that they appear transparent. After you upgrade version 13.00 or earlier to the latest version, your existing project's tags of invisible objects remain on scan. |
Provide Feedback