Options on the Hyperlink tab
The following table shows the options on the
Hyperlink
tab.Options | Descriptions |
|---|---|
Address | Specify the address that represents the linked destination. You can enter a URL address or a file path. You can also click Tag or Expression to specify a tag or an expression.An expression is a mathematical or logical equation that returns a value. A tag name can be used as an expression. |
Browse the Web | Click this button to open the default web browser on your computer. You can browse to the web page that you want to link to, and copy and paste the URL to the Address box.The URL must be enclosed in double quotes (" "). |
Browse for File | Click this button to select the file that you want to open at runtime. After you specify the file, the full path with the file name is shown in the Address box.The path must be enclosed in double quotes (" "). |
Provide Feedback