Assign function keys to objects
Use the
Key Assignments
option on the display's context menu to assign function keys to graphic objects. When the operator presses the function key at runtime, the object is activated.
TIP:
- You can assign the function keysF1throughF14, andK1throughK20.
- The list shows all the objects in the graphic display to which a function key can be assigned. If keys have already been assigned to the objects, the key name appears in brackets after the object name.
- You can also open theKey Assignmentsdialog box from theEditmenu.
To assign a function key to a graphic object
- Right-click the mouse in the display to open the context menu.
- ClickKey Assignmentsto open theKey Assignment Propertiesdialog box.
- In theSelect an objectbox, select the object. Only those objects in the display that can have keys assigned to them appear in the box.
- In theSelect a key assignmentbox, select the key to use. The assigned function key name appears in brackets after the object name in theSelect an objectbox.
- Repeat for as many keys as you want to assign.
- ClickOKto close the dialog box.
To change the function key assigned to a graphic object
- Right-click the mouse in the display to open theContextmenu.
- ClickKey Assignmentsto open theKey Assignment Propertiesdialog box.
- In theSelect an objectbox, select the object.
- In theSelect a key assignmentbox, select a new key orUnassigned.
- ClickOKto close the dialog box.
Key combination equivalents
If your keyboard does not have more than 12 function keys, you can use the following key combinations to simulate the other keys. If your keypad terminal does not have a
Right-Shift
key, attach a keyboard with a Right-Shift key to enable keys K13-K20
.For this function key assignment | Press this combination of keys |
|---|---|
F13 | Left SHIFT + F1 |
F14 | Left SHIFT + F2 |
K1 | Right ALT + F1 |
K2 | Right ALT + F2 |
K3 | Right ALT + F3 |
K4 | Right ALT + F4 |
K5 | Right ALT + F5 |
K6 | Right ALT + F6 |
K7 | Right ALT + F7 |
K8 | Right ALT + F8 |
K9 | Right ALT + F9 |
K10 | Right ALT + F10 |
K11 | Right ALT + F11 |
K12 | Right ALT + F12 |
K13 | Right SHIFT + F1 |
K14 | Right SHIFT + F2 |
K15 | Right SHIFT + F3 |
K16 | Right SHIFT + F4 |
K17 | Right SHIFT + F5 |
K18 | Right SHIFT + F6 |
K19 | Right SHIFT + F7 |
K20 | Right SHIFT + F8 |
Provide Feedback