Options for spacing objects
The following table shows the options for spacing objects on the
Arrange
menu.This option | Shifts objects |
|---|---|
Space Vertical | So the center points of each object are the same vertical distance from one another. The top and bottom objects do not move, but the other objects move up or down so there is equal space between the centers of each object. |
Space Horizontal | So the center points of each object are the same horizontal distance from one another. The left most and right most objects do not move, but the other objects move left or right so there is equal space between the centers of each object. |
Provide Feedback