Options for aligning objects
The following table shows the options for aligning objects on the
Arrange
menu. This option | Aligns objects to |
|---|---|
Align Left | left-most selected object |
Align Center | horizontal center of all selected objects |
Align Right | right-most selected object |
Align Top | top-most selected object |
Align Middle | vertical center of all selected objects |
Align Bottom | bottom-most selected object |
Align Center Points | center of all selected objects |
Align To Grid | grid |
Provide Feedback