Connections for the TerminalWakeUp ActiveX control

She following table shows the connections to control the operation of the TerminalWakeUp ActiveX control at runtime.
Connections
Descriptions
Event Trigger
Optional
When the assigned tag transitions from zero to non-zero, the control causes the
PanelView Plus 7
or
PanelView Plus 6
terminal to exit screen saver mode.
The connection can be a tag, a tag placeholder (for example, "{#1}"), or expression.
An application can use both triggers in the same control instance.
ChangeOfState Trigger
Optional
When the assigned tag changes state from the last triggering value, the control causes the
PanelView Plus 7
or
PanelView Plus 6
terminal to exit screen saver mode.
The connection can be a tag, a tag placeholder (for example, "{#1}"), or expression.
The initial triggering value is zero. The triggering value is not persisted between application (MER) execution, nor power cycles.
An application can use both triggers in the same control instance.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal