Connections for the SBCP ActiveX control
The following table shows the connections to control the operation of the SBCP ActiveX control at runtime.
Connections | Descriptions |
|---|---|
Select Required | When the tag value is non-zero, the control is active. When the tag value is zero (0), the control is inactive. When inactive, the Index connection value is persisted. The connection is read-only and can be a memory or direct reference tag. The connection data type is Analog. |
Index Required | When the control is active, the value of the configured tag determines which, if any, of the SBCP connections are set. When active:
The connection is read-only and can be a memory or direct reference tag. The connection data type is Analog. |
SBCP1 - SBCP100 Optional | These connections are the array of states associated with the PanelView Plus Enhanced SBCP object. When the control is active, the value of the Index connection determines which, if any, SBCP connection is set to one (1). Only one SBCP connection can be set to one (1) at a time. These connections are read-only and can be memory or direct reference tags. The connection data type is Analog or Boolean. |
Provide Feedback