Status connection values
The following table shows the values returned by the Status connection.
Values | Descriptions |
|---|---|
0x01 (Hex) or 1 (Dec) | Downloading |
0x02 (Hex) or 2 (Dec) | Download succeeded |
0x04 (Hex) or 4 (Dec) | Download with errors |
0x11 (Hex) or 17 (Dec) | Uploading |
0x12 (Hex) or 18 (Dec) | Upload succeeded |
0x14 (Hex) or 20 (Dec) | Upload with errors |
0x21(Hex) or 33 (Dec) | Deleting |
0x22(Hex) or 34 (Dec) | Delete succeeded |
0x24(Hex) or 36 (Dec) | Delete with errors |
Provide Feedback