ProgramParameter connection examples
The following table shows parameter examples you can follow when filling in the
ProgramParameter
connection.Parameters | Parameter Functions | Examples | Descriptions |
|---|---|---|---|
-p | Go to page | Foxitreader "file_path/file.pdf" -p 2 | Opens the PDF file to page 2. |
-zw | Fit width | Foxitreader “file_path/file.pdf” -zw | Opens the PDF file and fits the view to the page width. |
-zp | Fit page | Foxitreader “file.pdf”-zp | Opens the PDF file and shows the full page. |
-z | Zoom to | Foxitreader “file.pdf”-z 150 | Opens the PDF file and zooms to 150%. |
Multiple parameters | Enter empty spaces between parameters and parameter values | Foxitreader “file_path/file.pdf” -p 2 -zw | Opens the PDF file to page 2 and fits the view the page width. |
-b | Go to bookmark | Foxitreader “file_path/file.pdf” -b “Bookmark1” | Opens the PDF file to the location specified within Bookmark1. |
-d | Go to named destination | Foxitreader “file_path/file.pdf” -b “Destination1” | Opens the PDF file to the location specified within Destination 1. |
-g | Makes the File>Open command on the Menu and the Open folder button unavailable | Foxitreader “file_path/file.pdf” -g | Opens the PDF file and makes the Menu command File>Open and the Open folder button command unavailable. |
Provide Feedback