Connections for the MacroTen ActiveX control
The following table shows the connections to control the operation of the MacroTen ActiveX control at runtime. There are no additional parameters to configure the operation of the control beyond these connections.
Connections | Descriptions |
|---|---|
Enable Required | This connection is used to update all of the Write01 - Write10 properties. When the assigned value changes to a new non-zero value, this connection is triggered. The connection is read-only. The connection data type is Numeric. |
Read01 - Read10 Optional | These connections can be assigned to an expression, a tag, or a tag placeholder (for example, "{#1}"). Use these connections to read values that will be written to the Write01 - Write10 properties. The connection is read-only. The connection data type is Analog. |
Write01 - Write10 Optional | These connections can be assigned a tag or a tag placeholder. Use these properties to assign output tags from the Read01 - Read10 properties. The connection is write-only. The connection data type is Analog. |
Provide Feedback