ErrorMessage connection values
The following table shows the ErrorMessage connection values.
Error codes | Error messages |
|---|---|
0 | No error has occurred. |
1 | Operation is successful. |
2 | Operation has failed. Cannot get the interface to execute Macro. |
3 | Index property is out of range. Range is 1 to 100. |
4 | Macro_XX property has not been configured. |
5 | The macro configured in Macro_XX property does not exist. |
Provide Feedback