FailureCode connection values
The following table shows the FailureCode connection values returned by the EmailSender ActiveX control.
Error codes | Error messages |
|---|---|
1 (Dec) | Failed to start Winsock library. |
2 (Dec) | Windows socket library version is unsupported. |
3 (Dec) | Failure sending data over network. |
4 (Dec) | Failure receiving data over network. |
5 (Dec) | Failure connecting to remote server. |
6 (Dec) | Failed to get host name by address. |
7 (Dec) | Failure creating socket. |
8 (Dec) | Internal socket error. |
9 (Dec) | Internal socket error |
10 (Dec) | Invalid body file extension or format. |
11 (Dec) | Internal socket error. |
12 (Dec) | Bad SMTP user account. |
13 (Dec) | Internal error. Bad MD5 digest response. |
14 (Dec) | Internal error. Bad server name. |
15 (Dec) | Internal error. Server not responding. |
16 (Dec) | Internal error. Timeout occurred while communicating to the server. |
17 (Dec) | Memory allocation failure. System may be running out of memory. |
18 (Dec) | Failed to retrieve system time. |
19 (Dec) | Unexpected error. SMTP receive buffer found empty. |
20 (Dec) | Unexpected error. SMTP send buffer found empty. |
21 (Dec) | Connection to the server is closed while receiving data. |
22 - 33 (Dec) | Internal SMTP error. |
34 (Dec) | Authorization type not supported by the server. |
35 (Dec) | Internal SMTP error. |
36 (Dec) | Failure creating a thread. |
37 (Dec) | Specified attachment file is either missing or not accessible. |
38 (Dec) | Email TO recipient address is in invalid format. |
39 (Dec) | Email CC recipient address is in invalid format. |
40 (Dec) | Email BCC recipient address is in invalid format. |
41 (Dec) | Specified attachment file size exceeds the value defined in the AttachmentSize registry value. |
42 (Dec) | Specified Body File is either missing or not accessible. |
43 (Dec) | Failure opening specified body file. |
44 (Dec) | Sender email address is in invalid format. |
45 (Dec) | Internal ActiveX error. |
46 (Dec) | SMTP Server name is not specified. |
47 (Dec) | SMTP Server port is not specified. |
48 (Dec) | SMTP Server account username is not specified. |
49 (Dec) | SMTP Server account password is not specified. |
50 (Dec) | Email recipient address is not specified. |
51 (Dec) | Email sender address is not specified. |
52 (Dec) | Email queue is full. Maximum queue size limit is five emails. |
53 (Dec) | An error occurred while Unicode string conversion. |
54 (Dec) | SSL error occurred. |
55 (Dec) | SMTP error. Service unavailable. |
56 - 57 (Dec) | SMTP error. Recipient mailbox full. |
58 (Dec) | SMTP error. Recipient disk full. |
59 (Dec) | SMTP error. Recipient server not responding. |
60 (Dec) | SMTP error. Connection dropped during transmission. |
61 (Dec) | SMTP error. The maximum hop count was exceeded. |
62 (Dec) | SMTP error. Outgoing message timed out. |
63 (Dec) | SMTP error. Routing error. |
64 (Dec) | SMTP error. Requested action not taken: mailbox unavailable. |
65 (Dec) | SMTP error. Requested action canceled: local error in processing. |
66 (Dec) | SMTP error. Requested action not taken: insufficient storage. |
67 (Dec) | SMTP error. Syntax error, command unrecognized. |
68 (Dec) | SMTP error. Syntax error in parameters or arguments. |
69 (Dec) | SMTP error. Command not implemented. |
70 (Dec) | SMTP error. Bad sequence of commands. |
71 (Dec) | SMTP error. Command parameter not implemented. |
72 - 73 (Dec) | SMTP error. Bad Email Address. |
74 (Dec) | SMTP error. Recipient’ host server cannot be found. |
75 (Dec) | SMTP error. Domain does not accept mail. |
76 (Dec) | SMTP error. Access denied. |
77 (Dec) | SMTP error. SMTP login unsuccessful: bad username or password. |
78 (Dec) | SMTP error. Requested action not taken: mailbox unavailable. |
79 (Dec) | SMTP error. User not local, relay denied. |
80 (Dec) | SMTP error. Requested mail action canceled: exceeded storage allocation. |
81 (Dec) | SMTP error. Requested action not taken: mailbox name not allowed. |
82 (Dec) | SMTP error. Transaction failed. |
Provide Feedback