Options on the Advanced tab of the ME DataStore Plus Properties dialog box
The following table shows the options on the
Advanced
tab of the ME DataStore Plus Properties
dialog box.Options | Descriptions |
|---|---|
File Header | In the File Header area, there are the following options:
|
Log Periodically | Once the control is enabled, it logs periodically based on the time interval entered in this box. The time interval should be 1-9999s. |
Log System Time and Date of each record | Select this option to automatically record a System Time and Date stamp with each log entry. When logging System Time and Date, there is an option to also log a System Timezone Indicator. The indicator will contain the offset from UTC (Coordinated Universal Time) and the system's local timezone. Indicate Timezone When logging System time, this option adds a timezone indicator to the record. The system's Regional Setting determines the timezone offset. |
Log UTC Time and Date of each record | Select this option to automatically log a UTC Time and Date stamp with each record. |
Overwrite oldest data when file reaches | This option begins to overwrite the oldest data in the log file when the file reaches a specified size creating a circular log file. |
Log assigned connections only | This option optimizes the size of the log file by only logging configured connections. If this option is not selected, each record will always contain entries for 100 float and 50 string values. |
CSV File Logging Order | This option allows the designer to configure the order, in which data is written to the log file. |
Provide Feedback