Options on the General tab of the ME CSVDataLog Properties dialog box
The following table shows the options on the
General
tab of the ME CSVDataLog Properties
dialog box.Options | Descriptions |
|---|---|
Never | If this option is selected, the control will create a file named as your configuration. The control will use the file for all logging. |
Periodic | If this option is selected, the control will create a file using the naming convention YYYY_MM_DD_HH_MM_NNNN_<filename>.csv, for example, 2015_12_15_02_02_0001_File.csv.
If the Periodic option is selected, the following options are available:
|
At Specified Times | If this option is selected, the control will create a file using the naming convention YYYY_MM_DD_HH_MM_NNNN_<filename>.csv. In the Start Times text box, enter a time or times.
You can combine a time with a date or selected day of the week in the Start Times box. Enter times and dates in the format shown. Do not use time and date formats specific to the system's Regional Settings. |
Filename Delimiter Selection | This is a file format option allowing you to customize the filename.
|
Delete Oldest Files |
|
Provide Feedback