Options on the Pens tab of the ME ChartEx Control Properties dialog box
The following table shows the options on the
Pens
tab of the ME ChartEx Control Properties
dialog box.Options | Descriptions |
|---|---|
Display Legend | Select this check box to show the legend on the right of the chart. The legend percentage supports five percent increment from 10 percent through 50 percent. The legend shows each visible trend line with its label. The label is read from tags DataSeries_x.Label. |
Pen Attributes | Use the spreadsheet to configure the appearance of each pen on the chart at runtime, including line color, width, style, and marker. |
Color | Specify the color of the chart line. Click the color square and select a color from the palette. |
Width | Specify the width of the chart line. The larger the size, the thicker the width. |
Style | Specify the style of the chart line such as solid, dashed, dotted, and other styles. |
Marker | Specify the plot symbol for each data point. |
Connection Type | Select an option to specify how data points are connected for each pen.
|
Multiple Pen Edits | Use the spreadsheet to apply attributes to one or more pens. |
Clear Selections | Click this button to clear the attributes. |
Apply to Selected Pens | Click this button to apply the attributes to the selected pen or pens. |
Provide Feedback