Connections for the Chart and ChartEx ActiveX controls

The following table shows the connections for the Chart and ChartEx ActiveX controls.
Connections
Descriptions
Redraw
Required
This connection draws the chart object on each transition from zero to non-zero.
The connection is read-only.
The connection data type is Analog or Boolean.
Clear
Optional
This connection clears the chart area on each transition from zero to non-zero.
The connection is read-only.
The connection data type is Analog or Boolean.
Data_Source
Required
This connection contains the root tag of the chart UDT instance. The UDT must match the definition in the section
About User-defined Data Type
, otherwise, errors return.
The connection is read-only.
Tag placeholders are not supported.
ErrorCode
Optional
This connection allows the application to manage errors that occur with the chart control configuration.
The connection is write-only.
The connection data type is Integer.
ErrorMessage
Optional
This connection shows the text messages associated with
ErrorCode
.
The connection is write-only.
The connection data type is String.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal