Options in the Local Messages editor
The following table shows the options in the
Information Messages
editor.Options | Descriptions |
|---|---|
Trigger value | Type a non-zero integer trigger value. You can use positive and negative numbers. Trigger values do not need to be contiguous, but they must be unique for each message. For example, you could use trigger values of 1, 2, and 3, or values of 10, 20, and 30. The trigger value cannot be blank. |
Message | Do one of the following:
|
Provide Feedback