Options in the Time and Date Variable dialog box
The following table shows the options in the
Time and Date Variable
dialog box.Select this option from the list | To insert these characters | This format is called |
|---|---|---|
29/11/2000 | SD | Short date |
November 29, 2000 | LD | Long date |
29/11/2000 3:39:03 PM | SDT | Short date and time |
November 29, 2000 3:39:03 PM | LDT | Long date and time |
3:39:03 PM | T | Time |
3:39:03 PM 29/11/2000 | TSD | Time and short date |
3:39:03 PM November 29, 2000 | TLD | Time and long date |
Provide Feedback