Commands for detecting a CSV data log file
The following table shows the commands for detecting the integrity of a CSV data log file. The commands are case insensitive.
Commands | Descriptions |
|---|---|
ra_checkcsvintegrity -i file_path\file1.csv | file1 is the CSV file to be detected.The detection report will be shown in the Command Prompt window. |
ra_checkcsvintegrity -i file_path\file1.csv -o file_path\file2.txt | file1 is the CSV file to be detected.The detection report will be saved to file2 . |
ra_checkcsvintegrity -i file_path\*.csv | All the CSV files located at file_path\ will be detected.The detection report will be shown in the Command Prompt window. |
ra_checkcsvintegrity -i file_path\*.csv -o file_path\file2.txt | All the CSV files located at file_path\ will be detected.The detection report will be saved to file2 . |
ra_checkcsvintegrity ? | Show the instruction for the command lines in the Command Prompt window. |
Provide Feedback