Command examples for detecting a CSV data log file
The following table shows the command examples for detecting the integrity of a CSV data log file.
In the Command Prompt window, type | When press Enter |
|---|---|
ra_checkcsvintegrity -i c:\source\file.csv | The integrity of file.csv will be checked and the detection report will be shown in the Command Prompt window. |
ra_checkcsvintegrity -i c:\source\file.csv -o c:\report\file.txt | The integrity of file.csv will be checked and the detection report will be saved to file.txt . |
ra_checkcsvintegrity -i c:\source\*.csv | The integrity of all the CSV files at c:\source\ will be checked and the detection report will be shown in the Command Prompt window. |
ra_checkcsvintegrity -i c:\source\*.csv -o c:\report\file.txt | The integrity of all the CSV files at c:\source\ will be checked and the detection report will be saved to file.txt . |
Provide Feedback