Options in the New/Open Machine Edition Application dialog box
The following table shows the options in the
New/Open Machine Edition Application
dialog box.Options | Descriptions |
|---|---|
Application Name | The application name:
|
Description | The description can be up to 255 characters long. |
Language | Select a language for the application. The selected language will be the application's default language. |
Resolution | The Resolution list contains the same options as the Project window size list in the Project Settings dialog box, except the Custom size option. |
Provide Feedback