Open applications
Open an application when you start
FactoryTalk View Studio
or when FactoryTalk View Studio
is open.FactoryTalk View ME
application files are converted to the current version of FactoryTalk View
when you open them. Once the application has been converted, it cannot be opened by earlier versions of FactoryTalk View Studio
. However, you can still use the current version of FactoryTalk View Studio
to create runtime application files that will run on earlier versions of ME Station.If an application was created in earlier versions of
FactoryTalk View ME
, when you open the application in the current version of FactoryTalk View Studio
, ensure that the application's IP addresses do not contain a leading zero. FactoryTalk Linx
interprets a leading zero as an octal notation. For example, the IP address 131.200.13.111 is valid, but 131.200.013.111 is invalid. Before opening the application, edit the application's Nodes.csv file in Notepad by removing leading zeroes in IP addresses.To open an application in
FactoryTalk View Studio
, the logged-in user must have read/write access to the sub-folder that holds the HMI applications. If the security designation for FactoryTalk View Studio
users is Power Users, they may not have write access.To open an application
- IfFactoryTalk View Studiois not started, startFactoryTalk View Studio.
- IfFactoryTalk View Studiois started, from theFilemenu, selectOpen Applicationor click theOpen Applicationtool
. If an application is already open, FactoryTalk View Studioasks you whether to close the application that is currently open. ClickYes. - On theExistingtab, select the application to open.The resolution and version that was last used to open the application is shown.
- If the application has more than one language, select a language to open the application in.
- ClickOpen.
TIP:
To open two applications at the same time, for example to copy images and graphic objects between applications, start two instances of
FactoryTalk View Studio
.Provide Feedback