Switch application languages at design time
If an application is designed with multiple languages, you might want to switch application languages at design time to check the layout of translated text.
To switch application languages at design time
- From theApplicationmenu, selectChange Application Language, or on the toolbar, click
. - In theChange Application Languagedialog box, select the language you want to change to.TIP:The language list shows the languages added to the application, first with the language name and then with the language RFC1766 identification code.
- ClickOK.
The text in the following dialog boxes will be changed to the selected language:
- Alarm Setup
- Display
- Global objects
- Information Messages
- Local Messages
If any of the dialog boxes is opened and has unsaved changes, a message prompts you to save the changes.
Provide Feedback