Options in the Language Configuration dialog box
The following table shows the options in the
Language Configuration
dialog box.Options | Descriptions |
|---|---|
Add... | Click the Add button to open the Add Language dialog box where you can select a language to add to the application. |
Remove | Click the Remove button to remove the selected language from the list. A prompt appears asking you to verify that you want to delete the selection. When you click Yes , the selection is removed from the language list.If a language is the current language or the default language for the application, you cannot remove the language. |
Export... | Click the Export button to open the Export Operation dialog box of the String Import Export Wizard. |
Import... | Click the Import button to open the Import Operation dialog box of the String Import Export Wizard. |
Set As Default | To change the application's default language, select a language and click this button. A check mark appears beside the default language. |
Display undefined strings using the default language | Select this check box to show undefined strings for any language in the default language. If this check box is clear, undefined strings will be shown as single question mark characters (?). If a text string is undefined in the default language, it is shown as a single question mark. If you have specified that undefined strings will be shown in the default language, when you export strings to an Excel spreadsheet, undefined strings are exported as"**UNDEFINED**". However, when you export strings to a Unicode file, the default language strings will be exported for undefined strings. |
Provide Feedback