Options in the Import Operation dialog box
The following table shows the options in the
Import Operation
dialog box.Options | Descriptions |
|---|---|
Import strings from a Unicode text file into <RFC1766 Name> | Select this option to import strings for the language selected in the Language Configuration dialog box from a Unicode text file into the application. |
Import strings from an Excel spreadsheet into all application languages defined in the spreadsheet | Select this option to import text strings for all the application supported languages defined in the spreadsheet from an Excel spreadsheet into the application. |
Provide Feedback