Options in the Export Operation dialog box
The following table shows the options in the
Export Operation
dialog box.Table Heading | Table Heading |
|---|---|
Export strings for <RFC1766 Name> to one or more Unicode text files | Click this button to export the application's text strings for the language selected in the Language Configuration dialog box to a Unicode text file. |
Export strings for all languages to an Excel spreadsheet | Click this button to export the text strings for all the languages supported by the application to an Excel spreadsheet. |
Optimize duplicate strings | Select this check box to make sure the text strings that appear in the application more than once are written to the spreadsheet only once instead of every time they occur. |
Open exported file | Select this check box to open the exported file in Excel as soon as the export operation is completed. |
Provide Feedback