Options on the Runtime tab
The following table shows the options on the
Runtime
tab of the Project Settings
dialog box.Options | Descriptions |
|---|---|
Title bar | Select this check box to show the name of the project in the title bar at the top of the window. Type the name in the box below the check box. If you select this option, the window border is automatically shown with the title bar. |
Border | Select this check box to show a border around the project window. If you show the title bar, this option is selected automatically. You can clear the Border check box only if the Title bar check box is clear. |
Control box | Select this check box to show a control menu box in the upper left corner of the window. The user can click the control box to show the control menu, which contains options for manipulating the window. If you select this option, a Close button appears at the right end of the title bar.This option is available only if you select Title bar . |
Minimize button | Select this check box to show a Minimize button at the right end of the title bar. The Minimize button reduces the window to an icon.This option is available only if you select Title bar and Control box . |
Project window position | Type the number of pixels from the top left corner of the screen to position the project window. If the project window occupies the whole screen, accept the default values of 0. |
Enable auto logout | Select this check box to log out the current user automatically after the terminal is inactive for a specified period of time. |
Inactivity period | Specify the length of time (in minutes) the terminal must be inactive before the current user is automatically logged out and the default user is logged in. |
Return to graphic on logout | Select this check box to enable the application to navigate to a specified display when the current user is automatically logged out. If auto logout is active and this check box is clear, when the current user is logged out, the display was open at logout remains open.
|
Provide Feedback