Options on the Inactivity tab
The following table shows the options on the
Inactivity
tab of the Project Settings
dialog box.Options | Descriptions |
|---|---|
Enable advanced inactivity actions | Select this check box to enable the advanced inactivity actions. If this check box is clear, the other properties on the Inactivity tab are disabled. |
Log out the current user after an inactivity period | Select this check box to log out the current user automatically after the terminal is inactive for a specified period of time. If this check box is clear, the current user will not be logged out automatically. |
Inactivity period in minutes | Specify the length of time (in minutes) the terminal must be inactive before the current user is automatically logged out and the default user is logged in.
Parameter and expression are not supported. |
Navigate to a display after an additional delay | Select this check box to enable the application to navigate to a selected display when the terminal is inactive for a specified period of time since the current user is automatically logged out. If auto logout is active and this check box is clear, when the current user is logged out, the display was open at logout remains open. |
Additional inactivity period in minutes | Specify the length of time for which the terminal is inactive since the current user is automatically logged out before the application navigates to a specified display. Specify Literal value (0-32767 minutes), or Controlled by tag . |
Navigate to display | Select the display that the application navigates to after the additional inactivity period.
|
Inactivity time remaining (secs) | (Optional) Specify a numeric tag to read the remaining inactivity time in seconds. Click the browse button to open the Tag Browser and select the tag.Parameter and expression are not supported. |
Inhibit inactivity actions | (Optional) Specify a numeric tag to stop the inactivity actions from occurring indefinitely, and reset the inactivity timeout. Click the browse button to open the Tag Browser and select the tag.Parameter and expression are not supported.
|
Provide Feedback