Options in the application Properties dialog box
The following table shows the options on the
General
tab of the application Properties
dialog box.Options | Descriptions |
|---|---|
Name | This is the name specified on the New tab of the New/Open Machine Edition Application dialog box when the application was created. It cannot be changed here. |
Description | This is the description specified on the New tab of the New/Open Machine Edition Application dialog box when the application was created. You can change this description at any time |
Provide Feedback