FactoryTalk Linx or RSLinx Enterprise conversion log and shortcut validation
    The communications configuration (topology) on your workstation may be different from the configuration that was in use when the runtime application (.mer) was generated. Converting the runtime application to a different topology has the same effect as changing the shortcut device assignments. Failure to verify shortcut design assignments before using the converted application may result in unexpected behavior in the equipment being controlled. Confirm the design path and offline tag file assignments for each shortcut.
Provide Feedback