Rename an application
Use this dialog box to rename an application.
TIP:
If you want to rename a 7.0 or earlier version of application, convert the application to current version in
FactoryTalk View Studio
before the operation.You will not be prompted to validate user rights.
To rename an application
- SelectRename an applicationand clickNext.
- From the list, select the application you want to rename, and then clickNext.
- Type the new name of the application and clickFinish.
If the new name is the same as an existing application, an error message will appear. If the name is valid, the operation will proceed.
TIP:
When you enter a new application name, do not exceed 32 characters. If the application name exceeds the maximum 32 characters allowed by
FactoryTalk View Studio
, errors and warning messages will show.Provide Feedback