Options in the Edit Unit dialog box
The following table shows the options in the
Edit Unit
dialog box.Options | Descriptions |
|---|---|
Unit name | Shows the name of the unit selected on the Units tab. You can change this name to any name that is not in use in the recipe.This string does not allow runtime language switching. |
Select a data set | Shows the data set for the selected unit. Click the down arrow to open the list of data sets in the recipe file. Click a data set to select it and write its name into the data set field. |
Select a tag set | Shows the tag set for the selected unit. Click the down arrow to open the list of tag sets in the recipe file. Click a tag set to select it and write its name into the tag set field. |
Provide Feedback