Options in the Show / Hide Columns dialog box
The following table shows the options in the
Show / Hide Columns
dialog box.Options | Descriptions |
|---|---|
Select columns to show | Select the check boxes of the columns you want to show on the Ingredients tab.Clear the check boxes of the columns you want to hide on the Ingredients tab.By default, all the check boxes are selected. |
Show All | Click this button to select all the check boxes to show all the columns. |
Hide All | Click this button to clear all the check boxes to show all the columns. |
Show All Data Sets | Click this button to select the check boxes for all the data set columns. |
Hide All Data Sets | Click this button to clear the check boxes for all the data set columns. |
Show All Tag Sets | Click this button to select the check boxes for all the tag set columns. |
Hide All Tag Sets | Click this button to clear the check boxes for all the tag set columns. |
Provide Feedback